This document uses the following
conventions.
- Hexadecimal numbers can be
shown with the suffix h or the prefix 0x. For example, the following number
is 40 hexadecimal (decimal 64): 40h or 0x40.
- Registers in this document
are shown in figures and described in tables.
- Each register figure
shows a rectangle divided into fields that represent the fields of
the register. Each field is labeled with its bit name, its beginning
and ending bit numbers above, and its read/write properties with
default reset value below. A legend explains the notation used for
the properties.
- Reserved bits in a
register figure can have one of multiple meanings:
- Not
implemented on the device
- Reserved for
future device expansion
- Reserved for
TI testing
- Reserved
configurations of the device that are not supported
- Writing nondefault
values to the Reserved bits could cause unexpected behavior and
should be avoided.