SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The following section applies only to time-converted measurements; calibration for relative-time measurements is not required. All values captured by the HRCAP submodule are in number of HRCLK cycles. The HRCLK speed varies widely with temperature and voltage, thus a scale factor is required to convert the capture value to the SYSCLK domain. For the same reason, periodically recalculate the scale factor. The HRCAP submodule has a calibration block to reduce software overhead when calculating a scale factor between HRCLK and SYSCLK.
The calibration block contains the following key resources:
The calibration logic consists of two free-running counters; one clocked by HRCLK(HRCLKCTR) and one clocked by SYSCLK(HRSYSCLKCTR). When HRSYSCLKCTR is equal to HRCALIBPERIOD, the calibration block captures and resets both counter values, then triggers an interrupt, indicating a new scale factor is ready to be calculated. The scale factor can be found by dividing HRSYSCLKCAP by HRCLKCAP (see Equation 19). A DriverLib function, HRCAP_getScaleFactor, has been provided to determine the scale factor. This function can be called inside of the calibration interrupt service routine. If one of the counters experiences overflow, the CALPRDCHKSTS flag is set. The full details of the calibration block are described in Figure 22-2.