SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The external host interrupts the device using H2DINT that goes to the PIE. A write to the HICH2DTOKEN register triggers H2DINT. The H2DINT sources are shown in Figure 14-4.
The device interrupts the external host using D2HINT that comes out on a pin. A write to the HICD2HTOKEN register triggers D2HINT. The D2HINT sources are shown in Figure 14-5.
D2HINT can also be triggered by peripherals in the device (EVTRIG) as indicated in Figure 14-5. The sources for EVTRIG are listed in Table 14-2.
Event Trigger | Peripheral Interrupt Source |
---|---|
EVTRIG[0] | FSIRX_INT1, FSIRX_INT2 |
EVTRIG[1] | FSITX_INT1, FSITX_INT2 |
EVTRIG[2] | SPIB_TX, SPIB_RX |
EVTRIG[3] | SPIA_TX, SPIA_RX |
EVTRIG[4] | EPWM2, EPWM2_TZ |
EVTRIG[5] | EPWM1, EPWM1_TZ |
EVTRIG[6] | CLB2 |
EVTRIG[7] | CLB1 |
EVTRIG[8] | CLB4 |
EVTRIG[9] | CLB3 |
EVTRIG[10] | DMA Transfer |
EVTRIG[11..15] | Reserved |