SPRUIX1B October 2022 – April 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
FILE: can_ex8_mask.c
This example initializes CAN module A for Reception. When a frame with a matching filter criterion is received, the data is copied in mailbox 1 and LED is toggled a few times and the code gets ready for the next frame. If a message of any other MSGID is received, an ACK is provided Completion of reception is determined by polling CAN_NDAT_21 register. No interrupts are used. Refer to Programming Examples and Debug Strategies for the DCAN Module for useful information about this example
Hardware Required
Watch Variables