SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
The internal temperature sensor measures the junction temperature of the device. The output of the sensor can be sampled with the ADC through an internal connection. This can be enabled on channel ADCIN12 on ADCC and on the CMPSS2_HP5 input by setting the ENABLE bit in the TSNSCTL register.
To convert the temperature sensor reading into a temperature, pass the temperature sensor reading to the ADC_getTemperatureC() function in the ADC driverlib.