SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
FILE: dcc_ex1_single_shot_verification.c
This program uses the XTAL clock as a reference clock to verify the frequency of the PLLRAW clock.
The Dual-Clock Comparator Module 0 is used for the clock verification. The clocksource0 is the reference clock (Fclk0 = 20Mhz) and the clocksource1 is the clock that needs to be verified (Fclk1 = 120Mhz). Seed is the value that gets loaded into the Counter.
Please refer to the TRM for details on counter seed values to be set.
NOTE: In this device, by default, the XTAL is disabled and INTOSC2 is configured as the PLL source. To use XTAL (of frequency 20MHz) as the PLL source, update the device.h file with following changes :
To run this example, XTAL needs to be enabled. XTAL is enabled if you use it as the PLL source. You can also enable it by using the function SysCtl_turnOnOsc(SYSCTL_OSCSRC_XTAL)
External Connections
Watch Variables