SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
The ERRORSTS pin is an ‘always output’ pin and remains high until an error is detected inside the chip. On an error, the ERRORSTS pin goes low (default polarity) until the corresponding internal error status flag for that error source is cleared. Figure 4-4 shows the functionality of the ERRORSTS pin.
The ERRORSTS pin is tri-stated until the chip power rails ramp up to the lower operational limit. As the ERRORSTS pin is an active-low pin (default polarity), users who care about the state of this pin during power-up can connect an external pull-down on this pin.
Following enhancement has been made on this device for ERRORSTS pin logic: