SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
Table 5-3 describes the general boot ROM procedure each time the CPU core is reset.
During boot, boot ROM code updates a boot status location in RAM that details the actions taken during this process. Refer to Section 5.7.11 for more details.
Step | CPU Action |
---|---|
1 | After reset, perform watchdog initialization |
2 | Clock configuration and Flash power-up |
3 | Peripheral trimming and device configuration registers are loaded from OTP. |
4 | On power-on reset (POR), all RAMs are initialized. |
5 | Non-maskable interrupt (NMI) handling is enabled and DCSM initialization is performed. |
6 | Device calibration is performed; trimming the specified peripherals with set OTP values. |
7 | Determine if polling the GPIO pins are needed for determining the boot mode and, if so, read the boot mode GPIO pins to determine the boot mode to run. |
8 | Based on the boot mode and options, the appropriate boot sequence is executed. Refer to Section 5.5.1 for a flow chart of the boot sequences. |