SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
Generally, the lowest channel in the lowest PIE group has the highest priority. An example of this is channels 1.1 and 2.1. Those two channels have the highest priority in the respective groups. If the interrupts for those two enabled channels happened simultaneously and provided there are no other enabled and pending interrupts, channel 1.1 is serviced first by the CPU with channel 2.1 left pending.
However, there are cases where channel priority supersedes group priority. This special case happens depending on which step the CPU is currently at in the Interrupt Entry Sequence (Section 4.5.3).
The following illustrates an example of this special case.
The CPU is about to service channel 2.3 and is currently going through the steps in the Interrupt Entry Sequence (Section 4.5.3).
Group priority is only maintained if no interrupts are currently being serviced, that is, the Interrupt Entry Sequence (Section 4.5.3) is not executing.