SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
The Comparator Subsystem (CMPSS) consists of analog comparators and supporting circuits that are useful for power applications such as peak current mode control, switched-mode power, power factor correction, voltage trip monitoring, and so forth.
This device contains two variants of the CMPSS module: CMPSS and CMPSS_LITE. These modules share a common architecture, but some features are supported only by the full CMPSS variant and not the CMPSS_LITE variant. Carefully note where the documentation indicates that these certain features are not supported by the CMPSS_LITE variant. Also note that the device data sheet indicates electrical characteristics for the two variants separately.
See the C2000 Real-Time Control Peripheral Reference Guide for a list of all devices with modules of the same type, to determine the differences between the types, and for a list of device-specific differences within a type.