SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
The required frequency tolerance for the CAN bit clock depends on the bit timing setup and network configuration, and can be as tight as 0.1%. Since the main system clock (in the form of SYSCLK) can not be precise enough, the bit clock can also be connected to XTAL using the CLKSRCCTL2 register. There is an independent selection for each CAN module.
To provide correct operation, the frequency of the CAN bit clock must be less than or equal to the SYSCLK frequency.