SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
Lockstep comparison is disabled automatically during debug/emulation mode of the device. However, some items are still available when a debugger is connected:
The status of the debugger connection is readable from the status register, specifically the LCM_REGS[LCM_STATUS.DBGCON] bit.
To re-initialize the lockstep compare module (after debugger is disconnected), a reset is required. This reset is called using a system reset requested from the debugger which in turn generates an XRSn in the device.