SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
If local shared RAM is configured as dedicated RAM for the CPU, or if the RAM is configured as data RAM for the CLA, any fetch access from the CLA to that particular LSx RAM results in a CLA fetch protection violation, which is a non-controller access violation.
If a CLA fetch protection violation occurs, the violation results in a MSTOP, a flag gets set into the appropriate access violation flag register, and the memory address for which the access violation occurred gets latched into the appropriate CLA fetch access violation address register. Also, an access violation interrupt is generated to the controller CPU if the interrupt is enabled in the interrupt enable register.