SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This section provides information for both single-bit data errors and single-bit ECC check bit errors. If there is a single bit flip (0 to 1 or 1 to 0) in Flash data or in ECC data, then the error is considered as a single-bit data error. The SECDED module detects and corrects single-bit errors, if any, in the 64-bit Flash data or eight ECC check bits read from the Flash/ECC memory map before the read data is provided to the CPU.
When SECDED finds and corrects single bit data errors, the following information is logged in the ECC registers if the ECC feature is enabled:
When the ERR_CNT value equals ERR_THRESHOLD+1, and a single bit error occurs, the Flash module sets the SINGLE_ERR_INT flag and generates an interrupt signal. To enable propagation of the generated interrupt pulse to the CPU, the user application must enable the FLASH_CORRECTABLE_ERROR channel in the C28 Peripheral Interrupt Expansion module (PIE). The interrupt signal remains high until the application clears the SINGLE_ERR_INTFLG flag by writing to the SINGLE_ERR_INTCLR bit in the ERR_INTCLR register. The Flash module cannot generate any further FLASH_CORRECTABLE_ERROR interrupt signals to the PIE/CPU until SINGLE_ERR_INTFLG is cleared, as this is an edge-based interrupt.
When multiple single-bit errors have been detected by ECC logic, the contents of the Flash ECC registers reflect the most recent ECC error. When multiple single-bit errors have been detected, both FAIL_0_L and FAIL_1_L (or FAIL_0_H and FAIL_1_H) can be set, indicating that single-bit fail0/fail1 occurred in different 64-bit aligned addresses.
Although ECC is calculated on 64-bit basis, a read of any address location within a 128-bit aligned Flash data word causes the single-bit error flag to get set, if there is a single-bit error in both or in either the lower 64 or upper 64 bits (or corresponding ECC check bits) of that 128-bit data word.