SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
MCU Configuration registers (MCUCNFx) have been implemented to enable customers to emulate a sub-set device on a super-set device. Table 3-15 shows the list of the available MCUCNF registers and the sub-set features that can be emulated. See the MCUCNFx register descriptions for more details. This feature only works when emulating a sub-set device on a super-set device but not the other way around.
Register | Feature to Modify |
---|---|
MCUCNF0 | Dual to Single core |
MCUCNF1 | D2 - D5 CPU1/CPU2 memory allocation |
MCUCNF2 | With EtherCAT to no EtherCAT |
MCUCNF3 | Flash Bank1 sector allocation if bank is present |
MCUCNF4 | Flash Bank2 sector allocation if bank is present |
MCUCNF5 | Flash Bank3 sector allocation if bank is present |
MCUCNF6 | Flash Bank4 sector allocation if bank is present |
MCUCNF7 | Flash Bank5 sector allocation if bank is present |