SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The CLB Input X-BAR is architecturally identical to the Input X-BAR. The only difference is the destination for each INPUTx. The destination for each INPUTx is only the CLB Tiles as shown in . This allows for GPIOs to be accessed by the CLB tiles without using the combination of Input X-BAR and CLB X-BAR.
INPUT | CLB | ETPWM X-BAR | ETPWM DEL |
---|---|---|---|
1 | Yes | - | Yes |
2 | Yes | - | Yes |
3 | Yes | - | Yes |
4 | Yes | - | Yes |
5 | Yes | - | Yes |
6 | Yes | - | Yes |
7 | Yes | Yes | Yes |
8 | Yes | Yes | Yes |
9 | Yes | Yes | Yes |
10 | Yes | Yes | Yes |
11 | Yes | Yes | Yes |
12 | Yes | Yes | Yes |
13 | Yes | Yes | Yes |
14 | Yes | Yes | Yes |
15 | Yes | - | Yes |
16 | Yes | - | Yes |