SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The CAN module provides several test modes that are mainly intended for self-test purposes. Figure 25-3 aids in understanding the various test modes. Figure 25-3 must be viewed as representative of the module behavior, and not as a gate-accurate implementation of the module. Figure 25-3 does not include the GPIO muxing or the I/O buffers.
For all test modes, the Test bit in the CAN control register needs to be set to 1 to enable write access to the CAN_TEST register.