SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The dual code security module (DCSM) is a security feature incorporated in this device. The DCSM prevents access and visibility to on-chip secure memories (and other secure resources) by unauthorized persons. The DCSM also prevents duplication and reverse-engineering of proprietary code. The term “secure” means that access to on-chip secure memories and resources is blocked. The term “unsecure” means that access is allowed; that is, the contents of the memory can be read by any means (for example, through a debugging tool such as Code Composer Studio™ IDE.
The CSM has dual-zone security: Zone1 (Z1) and Zone2 (Z2).