SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
If additional time between samples is desired, the application can configure SPREAD equal to the number of SYSCLK cycles desired between samples. Figure 18-9 shows an example of oversampling from an ePWM trigger with a 500-cycle spread between samples.
TRIGGER = ePWM SOCA, NSEL = 3, MODE = Oversampling, PHASE = 0, SPREAD = 500
Figure 18-9 ADC Repeated Trigger Example with Sample Spread