SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
In systems that do not require the redundant module for functional safety requirements, the LCM redundant module can be disabled for additional power savings. To disable the LCM comparators upon device startup or after reset, the following steps must be taken at the beginning of the user application code:
Note: The redundant lockstep module is disabled by this write and cannot be re-enabled without a reset.