SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Distributed clocks (DC) allows the tracked time at ESC be synchronized across the EtherCAT network, which makes precisely timed events possible throughout the network. Events can be realized with triggers from ESC outputs that are programmed to create a toggle at a certain absolute time tracked by the ESC or through sampling of timestamp of certain system event inputs to ESC that can further be used for synchronizing the time.