SPRUJ17H March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The ALE sends per port statistics along with the frame routing to be counted in the CPSW statistics. There are multiple reasons that frames are dropped by the ALE. Each drop is counted in the CPSW statistics. For more information on ALE statistics refer to the CPSW Network Statistics section.