All interrupts and events
generated by the R5FSS are summarized in R5FSS
Integration, along with their mapping. These
processor events can be divided into the following groups:
- R5F CPU internal interrupts and events: these include the R5 EVENT signals and PMU interrupts. These are described in the Arm Cortex-R5 Technical Reference Manual.
- ECC аggregator interrupts: only VIM memory errors generate the interrupt. These are described in the ECC Aggregator chapter.
- TCM Address parity Error Interrupts: these are described in the TCM Address Parity Error section.
- Lockstep Compare Interrupts: these are described in the Lockstep Compare section.
- Selftest Logic Interrupt: interrupts and errors generated by selftest logic. These are described in the Selftest Controller (STC) chapter.