SPRUJ17H March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
Trigger Input Bit | Source Signal | Comments |
---|---|---|
[7] | Reserved | |
[6] | Reserved | |
[5] | Reserved | |
[4] | Reserved | |
[3] | Reserved | |
[2] | STM:ASYNCOUT | Alignment synchronization output. The STM asserts this signal for one clock cycle when an ASYNC-VERSION-FREQ sequence is output on the ATB interface, and the ASYNCOUT signal can be used for cross-triggering. |
[1] | STM:TRIGOUTSW | The STM asserts this signal for one clock cycle when a trigger event is generated on writes to a TRIG location in the extended stimulus port registers |
[0] | STM:TRIGOUTSPTE | The STM asserts this signal for one clock cycle when a trigger event is detected on a match using the STMSPTER. |