SPRUJ17H March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The Cortex-R5F is a processor from Arm, which is based on the Armv7-R profile. Each R5FSS implements two R5F cores, CPU0 and CPU1, each with their own RAMs and interfaces. While in reset, they can be bootstrapped to work in one of two modes: Dual Core or Lockstep.
In dual core mode, each R5F core works completely independent from the other (asymmetric multiprocessing, or AMP). Each core uses its own RAMs and interfaces, with no coherence between the two cores.
In Lockstep mode:
For a brief list of features supported by the R5F processor in this device, see R5FSS Features. For more detailed description of this processor, see the Arm Cortex-R5 Technical Reference Manual.