The AWR2944EVM/AWR2944PEVM can be
connected to the DCA1000 EVM platform to allow for LVDS data streaming.
Figure 2-25 shows the AWR2944EVM/AWR2944PEVM interfaced to the DCA1000 EVM.
When using the AWR2944EVM/AWR2944PEVM
with the DCA1000 EVM, the following settings must be used.
- Set the AWR2944EVM/AWR2944PEVM to
SOP2 mode.
- Set the
DCA1000 EVM switches to the following configuration.
- The 12V supply must be connected
to J12 on the AWR2944EVM/AWR2944PEVM.
- A 5V supply must be connected to
J2 on the DCA1000 EVM.
- A micro USB cable must be
connected to the FTDI port on the AWR2944EVM/AWR2944PEVM (J10).
- The Samtec ribbon cable must be
connected to J7 on the AWR2944EVM/AWR2944PEVM and J3 on the DCA1000 EVM.
- An RJ45 cable must be connected
to J6 on the DCA1000 EVM.