LAUNCHXL-F280039C is a low-cost development board for the TI C2000
real-time microcontrollers series of F28003x devices. This LaunchPad™ kit offers
extra pins for development and supports the connection of two BoosterPack™
plug-in modules.
- The hardware files are in the
<install_location>\boards\LaunchPads\LAUNCHXL_F280039C
folder of C2000Ware.
- For more details about the LAUNCHXL-F280039C, see the C2000™ F28003x
Series LaunchPad™ Development Kit User's Guide.
- Make
sure that the switches on the LAUNCHXL-F280039C are set as described below shown in Figure 3-2.
- Install jumpers on JP1,
JP2 and J101 for the power supply and debug JTAG. And install jumpers on
JP8 for the power supply of DAC128S board if used.
- For S2, position
the SEL1 (LEFT) switch UP (1) to route GPIO28 and GPIO29 to the
BoosterPack connector, and position the SEL2 (RIGHT) switch UP
(1) to rout GPIO15 and GPIO56 to the virtual COM port of the XDS110
debugger.
- For S3, position
the GPIO24 (LEFT) switch DOWN to pull GPIO24 low to logic 0, and
position the GPIO32 (RIGHT) switch UP to pull GPIO32 high to
logic 1 to put the F280039C into wait boot mode to reduce the risk of
connectivity issues or a previous loaded code execution.
- For S4, set S4 to
DOWN (on) to route GPIO4 and GPIO5 to the CAN transceiver
interface J14 if the pre-define symbol "CMD_CAN_EN" is set in the
project properties. Set S4 to UP (off) to route GPIO4 and GPIO 5
to the BoosterPack connectors otherwise.
- For S5, position
the QEP1 SEL (LEFT) switch DOWN to route GPIO40/41/59 to the
eQEP1 encoder interface on J12 and position the QEP2 SEL (RIGHT) switch
DOWN to route GPIO14/55/57 to the eQEP2 Hall sensor interface
on J13.