- Power on the AC or DC power
supply, gradually increase output voltage at power supply to get an appropriate
DC-bus voltage.
- Run the project by clicking on
button
, or click Run → Resume in the Debug
tab. The systemVars.flagEnableSystem should be set to '1' after a
fixed time, that means the offsets calibration have been done. The fault flags
motorVars_M1.faultMtrUse.all should be equal to '0' , if not,
the user have to check the current and voltage sensing circuit as described in
Section 3.5.1.
- To verify run the motor with
current closed-loop control, set the variable
motorVars_M1.flagEnableRunAndIdentify to '1' in the
Expressions window as shown in Figure 3-43. The motor will run with a closed-loop control using the angle from the angle
generator at a setting speed in the variable motorVars_M1.speedRef_Hz.
Check the value of motorVars_M1.speed_Hz in Expressions window, The
values of both variables should be very close.
- Connect oscilloscope probes to
the EPWMDAC or DAC128S outputs and motor phase line to probe the angles and
current signals, and current. These waveforms on the oscilloscope appear as
shown in Figure 3-44. Change the motorVars_M1.Idq_set_A.value[1] in the Expressions
window to set the reference torque current, the motor phase current will be
increasing with the same percentage accordingly.
- If the motor cannot run with
current-closed loop control and an over current fault appears, check if the sign
of motorVars_M1.adcData.current_sf and the value of
userParams_M1.current_sf are set correctly according to the hardware
board. The values of both variables are related to the definition constant
USER_M1_ADC_FULL_SCALE_CURRENT_A in the user_mtr1.h file.
- Set the variables
motorVars_M1.flagEnableRunAndIdentify to 0 to stop run the
motor.
- Once complete, the controller can
now be halted and the debug connection terminated. Fully halting the controller
by first clicking the Halt button
on
the toolbar or by clicking Target → Halt. Finally, reset the
controller by clicking on
or
clicking Run → Reset.
- Close CCS debug session by
clicking on Terminate Debug Session
or
clicking Run → Terminate.
Use DAC128S085EVM with an oscilloscope to monitor rotor angle of the motor
from the angle generator and rotor angle from the FAST estimator, and a phase
current of the motor as shown in Figure 3-44.