SPRUJ40C may 2022 – may 2023
Applicable EVM Revisions: E1, E2
Issue Description: The OLDI Connector Pinout was updated after version E2 in order to improve the differential routing on the cable. Please refer to Section 2.6.3 for the pinout change details.
Important Note: An adapter is required in order to enable E1 & E2 boards to connect to the TI recommended OLDI displays. DO NOT ATTEMPT to plug in an E1 or E2 board into such an LCD without the adapter.