SPRUJ42E March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
PRODUCTION DATA
Enet Port N FIFO STATUS
Return to Summary Table
Offset = Base + (k * 1000h); where k = 0 to 1d
Instance Name | Physical Address |
---|---|
CPSW0 | 5282 2050h + formula |
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
NONE | |||||||
0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | EST_BUFACT | EST_ADD_ERR | EST_CNT_ERR | ||||
NONE | R | R | R | ||||
0h | 0h | 0h | 0h | ||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
TX_E_MAC_ALLOW | |||||||
R | |||||||
FFh | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
TX_PRI_ACTIVE | |||||||
R | |||||||
0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31:19 | RESERVED | NONE | 0h | Reserved |
18 | EST_BUFACT | R | 0h | EST RAM active buffer - Indicates the active 64-word fetch buffer when pn_est_onebuf is cleared to zero. Indicates the fetch ram address MSB when pn_est_onebuf set to one. |
17 | EST_ADD_ERR | R | 0h | EST Address Error - Indicates that the fetch ram was read again after the previous maximum buffer address read (the previous fetch from the maximum address is reused). |
16 | EST_CNT_ERR | R | 0h | EST Fetch Count Error - Indicates that insufficient clocks were programmed into the fetch count and that another fetch was commanded before the previous fetch finished. |
15:8 | TX_E_MAC_ALLOW | R | FFh | Transmit mac allow - Bus that indicates the actual priorities assigned to the express queue (and inversely the priorities assigned to the prempt queue). The pn_mac_prempt[7:0] field in the Enet_Pn_IET_Control register indicates which priorities should be assigned to the express/prempt queues. The switch between queues happens only when the priority is empty and the actual assignment is shown in this field. |
7:0 | TX_PRI_ACTIVE | R | 0h | Transmit Priority Active - Bus that indicates which priorities have packets (non-empty) at the time of the register read. |