SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: mcan_ex8_range_filter_receive.c
This example demonstrates Receiving, with RANGE filter configuration. The transmitting node could be a CAN FD capable controller or a CAN bus analysis tool capable of transmitting CAN FD frames. Only Extended IDs from 0x1FFFFF23 to 0x1FFFFF46 are received. Other IDs are not received. RXFIFO1 starts at an offset of 748 (2EC). MCAN Message RAM starts at 0x58000, so received messages will be copied starting at address 0x582EC. Note that as long as the ID matches, "classic" CAN frames will also be received.
The transmit and receive pins of the MCAN module should be connected to a CAN Transceiver. Nominal Bit Rate of 500 kbps and Data bit rate of 1 Mbps is used.
Hardware Required
External Connections
Both nodes should communicate through CAN FD capable transceivers.
Watch Variables