SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
This sections gives details about the entry point addresses for various boot modes. These entry points direct the boot ROM what address to branch to at the end of booting as per the selected boot mode.
Table 4-22 gives the entry point addresses for Flash boot mode.
Table 4-18 gives the entry point addresses for RAM boot mode.
Option | BOOTDEFx Value | Flash Sector | Address | Devices Supported |
---|---|---|---|---|
0 | 0x03 | Bank 0 Sector 0 | 0x0008 0000 | All |
1 | 0x23 | Bank 0 Sector 32 | 0x0008 8000 | All |
2 | 0x43 | Bank 2 Sector 0 | 0x000C 0000 | All |
3 | 0x63 | Bank 2 Sector 32 | 0x000C 8000 | All |
4 | 0x83 | Bank 4 Sector 0 | 0x0010 0000 | Device Dependent |
Option | BOOTDEFx Value | RAM Entry Point | Package Supported |
---|---|---|---|
0 | 0x05 | 0x0000 0000 | All |