SPRUJ53B April 2024 – September 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: fsi_ex5_periodic_frame.c
Example sets up infinite data frame transfers where trigger comes from ISR handling the periodic CPU Timer event. Automatic(Hw triggered) Ping frame transmission is also setup along with data.
CPU Timer0 is chosen for setting up periodic timer events. User can choose any other Timer-1/Timer-2 as well.
Automatic(Hw triggered) Ping frame transmission is also setup along with data.
If there are any comparison failures during transfers or any of error event occurs, execution will stop.
External Connections
For FSI internal loopback (EXTERNAL_FSI_ENABLE == 0), no external connections needed
For FSI external loopback (EXTERNAL_FSI_ENABLE == 1), external connections are required. The FSI TX pins should be connected to the respective FSI RX pins of the same device. See below for external connections to include and GPIOs used:
External Connections Required between FSI TX and RX of the same device:
ControlCard FSI Header GPIOs:
Watch Variables