SPRUJ53B April 2024 – September 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: sci_ex1_loopback.c
This program uses the internal loop back test mode of the peripheral. Other then boot mode pin configuration, no other hardware configuration is required. The pinmux and SCI modules are configured through the sysconfig file.
This test uses the loopback test mode of the SCI module to send characters starting with 0x00 through 0xFF. The test will send a character and then check the receive buffer for a correct match.
This example project has support for migration across our C2000 device families. If you are wanting to build this project from launchpad or controlCARD, please specify in the .syscfg file the board you're using. At any time you can select another device to migrate this example.
Watch Variables