SPRUJ53B April 2024 – September 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: cla_ex2_atan.c
In this example, Task 1 of the CLA will calculate the arctangent of an input argument using a lookup table.
Note that since this example does not use background CLA task, the compile flag cla_background_task is turned off for this project. Set this flag as on to enable background CLA task. The option is available in Project Properties -> C2000 Build -> C2000 Compiler -> Advanced Options -> Runtime Model Options.
Memory Allocation
Watch Variables