SPRUJ53B April 2024 – September 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: mcan_ex15_timestamp.c
This example demonstrates the MCAN Timestamping functionality. When the TRANSMIT define is selected, the CAN Controller acts as a Transmitter and sends data to the second CAN Controller connected externally. If TRANMSIT is not defined the CAN Controller acts as a Receiver and waits for message to be transmitted by the External CAN Controller.
External Connections
Watch Variables