If the clock to the CMPSS module is disabled while
the comparator is active, the following behavior can be expected:
- The comparator remains
unaffected and continues to trip from voltages on the inputs.
- If the reference 12-bit DAC
is driving the negative input of the comparator, the voltage on the negative
input remains static and unaffected but DACVALA can no longer be updated
from the ramp generator or DACVALS.
- The ramp generator,
synchronize block and digital filter freeze on the current states.
Enabling the clock to the CMPSS
restores the clock to the state before the clock was disabled.