SPRUJ62 December 2022 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
Dip switches [SW2] [SW4] [SW13] [SW16] are used to configure different options available on the EVM.
[SW2] Position |
Default | Function | Description |
---|---|---|---|
SW2.1 | OFF | Octal-SPI Memory Selection |
MUX to select between non-volatile Octal-SPI memory connected to the MCU_OSPI0 interface: ‘0’ (OFF) = xSPI Memory is selected ‘1’ (ON) = Octal-NAND is selected |
SW2.2 | ON | Debug/Trace Enable |
MUX to select between Debug/Trace (connected via MIPI 60 emulation interface) and variety of ‘other’ EVM features (1): ‘0’ (OFF) = ‘Other’ EVM features are selected/enabled ‘1’ (ON) = Debug/Trace is enabled to MIPI-60 emulation interface |
SW2.[4:3] | OFF:OFF | USB Type C Mode Selection |
Set Mode for USB Type C interface (USB0): '00' (OFF/OFF) = DFP (Downstream Facing Port) ‘01’ (OFF/ON) = DRP (Dual Role Port) ‘1X’ (ON, Don’t Care) = UFP (Upstream Facing Port) |
SW2.5 | OFF | PCIe0 Mode Selection |
Set Mode for PCIe0 (4-Lane) ‘0’ (OFF) = Root Complex ‘1’ (ON) = End Point |
SW2.6 | OFF | PCIe1 Mode Selection |
Set Mode for PCIe1 (2-Lane) ‘0’ (OFF) = Root Complex ‘1’ (ON) = End Point |
SW2.7 | ON | IO Voltage for Serial Camera Add-on Board(s) |
Configures IO supply for Serial Camera Expansion Interface (I2C, GPIO, etc). Voltage levels of CSI2-RX signals is defined by MIPI specification. ‘0’ (OFF) = IO Levels are set to 3.3VDC ‘1’ (ON) = IO Levels are set to 1.8VDC |
SW2.8 | ON | Reserved |
Reserved for future feature enhancement. Must be set to ‘1’ (ON) for EVM to function correctly. ‘0’ (OFF) = Invalid setting ‘1’ (ON) = Must be set to ‘1’ |
SW2.9 | ON | EVM Configuration EEPROM Write Protection |
Sets EVM’s configuration EEPROM Write Protection ‘0’ (OFF) = Configuration EEPROM can be updated ‘1’ (ON) = Configuration EEPROM cannot be updated/is protected |
SW2.10 | ON | User Defined |
User Defined, maps to GPIO/IO Expander Input (See GPIO tables) ‘0’ (OFF) = User Defined ‘1’ (ON) = User Defined |
SW13.1 | OFF | LIN1 Mode Selection |
Configure Master/Slave mode for LIN1 Interface ‘0’ (OFF) = Slave Mode ‘1’ (ON) = Master Mode |
SW13.2 | OFF | LIN2 Mode Selection |
Configure Master/Slave mode for LIN2 Interface ‘0’ (OFF) = Slave Mode ‘1’ (ON) = Master Mode |
Table 2-5 shows the J7AHP EVM configuration switches [SW4] [SW16] to set the various Power Management IC (PMIC) and reset functions.
[SW16] Position |
Default | Function | Description |
---|---|---|---|
SW4.1 | OFF |
Reserved / Test Mode (Wait Reset) |
Reserved, Must set to ‘0’ (OFF) for normal EVM operation (only used in Test Mode) |
SW4.2 | OFF |
Reserved / Test Mode (Wait Reset) |
Reserved, Must set to ‘0’ (OFF) for normal EVM operation (only used in Test Mode) |
SW16.1 | ON | Reserved / Tests Mode (PMIC Enable) |
Reserved, Must set to ‘1’ (ON) for normal EVM operation (only used in Test Mode) ‘0’ (OFF) = Disable PMIC (Do Not Use) ‘1’ (ON) = Enable PMIC |
SW16.2 | ON | Reserved / Test Mode (VMonitor Enable) |
Reserved, Must set to ‘1’ (ON) for normal EVM operation (only used in Test Mode) ‘0’ (OFF) = Disable Voltage Monitor (Do Not Use) ‘1’ (ON) = Enable Voltage Monitor |
SW16.3 | ON |
Reserved / Test Mode (Disable) |
Reserved, Must set to ‘1’ (ON) for normal EVM operation ‘0’ (OFF) = Enable Test Mode (Do Not Use) ‘1’ (ON) = Disable Test Mode |
SW16.4 | ON | Watchdog Disable |
Enable/Disable of Watchdog Timer within PMIC. (Note this can cause processor reset if watchdog is not managed.) ‘0’ (OFF) = Watchdog Timer is Enabled ‘1’ (ON) = Watchdog Timer is Disabled |