The recommended steps for using the F28P65x LaunchPad are:
- Follow the instructions in Section 2.2 to begin running the
LaunchPad demo program. Within just a few minutes, you can control and
monitor the F28P65x LaunchPad with the pre-programmed quick start application.
Additionally, the FAQ section included in this document can be helpful if there
are any issues that can quickly be addressed.
- Experiment with BoosterPacks. This
development kit conforms to the latest revision of the BoosterPack pinout
standard. This development kit has two independent BoosterPack sites to enable a
variety of expansion opportunities, such as two boosterpacks being used
simultaneously. For more information about the TI LaunchPad and BoosterPack
standard, see the TI LaunchPad.
- Take the first step towards developing your
own control applications. The F28P65x LaunchPad is supported by the
C2000Ware development package. After C2000Ware is installed, look
for \f28p65x\examples\c28x\launchxl_f28p65x in the installation directory to
find the pre-configured example applications for this board. Any of the other
examples found within the \f28p65x\examples directory can be used with minor
modifications to run on the LaunchPad as well. For more details about software
development, see Section 2.
- For applications,
features and benefits information, see the TMS320F28P65x Real-Time Microcontrollers.
- Check out this technical article featuring C2000 Real-Time
Microcontrollers about how developers can take advantage of
the scalability and sustainability benefits these devices bring.
- Customize and integrate the hardware to align to your end application. This development kit can be used as a reference for building your own custom boards and circuits based on C2000 F28P65x series microcontrollers. The LaunchPad also functions as a foundation for expansion with custom BoosterPacks and other circuits. This document can serve as a starting point for such projects.
- Get Trained. Review and download hours of written and video training materials on C2000 Real-time Microcontrollers and related LaunchPads.
- See Getting Started With C2000™ Real-Time ControlMicrocontrollers (MCUs)
- See the TI Training and Videos page
- See the C2000 Academy page