SPRUJ86C October   2023  – August 2024 AM263P2 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
      1.      Preface: Read This First
        1. 1.1.1.1 Sitara MCU+ Academy
        2. 1.1.1.2 Important Usage Notes
    2. 1.2 Kit Contents
    3. 1.3 Device Information
      1. 1.3.1 HSEC 180-pin Control Card Docking Station
      2. 1.3.2 Security
  6. 2Hardware
    1. 2.1  Component Identification
    2. 2.2  Power Requirements
      1. 2.2.1 Power Input Using USB Type-C Connector
      2. 2.2.2 Power Status LEDs
      3. 2.2.3 Power Tree
      4. 2.2.4 Power Sequence
      5. 2.2.5 PMIC
    3. 2.3  Functional Block Diagram
    4. 2.4  Reset
    5. 2.5  Clock
    6. 2.6  Boot Mode Selection
    7. 2.7  JTAG Path Selection
    8. 2.8  Header Information
    9. 2.9  GPIO Mapping
    10. 2.10 Push Buttons
    11. 2.11 Interfaces
      1. 2.11.1  Memory Interface
        1. 2.11.1.1 OSPI/QSPI
        2. 2.11.1.2 Board ID EEPROM
      2. 2.11.2  Ethernet Interface
        1. 2.11.2.1 Control Card Ethernet Routing
        2. 2.11.2.2 On Board Ethernet PHY
        3. 2.11.2.3 LED Indication in RJ45 Connector
        4. 2.11.2.4 Ethernet Add On Board Connector
      3. 2.11.3  I2C
      4. 2.11.4  Industrial Application LEDs
      5. 2.11.5  SPI
      6. 2.11.6  UART
      7. 2.11.7  MCAN
      8. 2.11.8  FSI
      9. 2.11.9  JTAG
      10. 2.11.10 Test Automation Header
      11. 2.11.11 LIN
      12. 2.11.12 MMC
      13. 2.11.13 ADC and DAC
    12. 2.12 HSEC Pinout and Pinmux Mapping
  7. 3Hardware Design Files
  8. 4Additional Information
    1. 4.1 If You Need Assistance
    2. 4.2 Trademarks
  9. 5Related Documentation
    1. 5.1 Supplemental Content
      1.      5.1.A E1 Board Modifications
      2.      5.1.B E2 Design Changes
      3.      5.1.C A Design Changes
  10. 6References
    1. 6.1 Reference Documents
    2. 6.2 Other TI Components Used in This Design
  11. 7Revision History
  12. 8Revision History

E1 Board Modifications

  1. OSPI Modification - Implemented to all E1 boards out-of-box.

    The initial design of the AM263Px Control Card E1 included a 2.5 inch stub hanging off of the OSPI DQ0 and DQ1 signal lines. These stubs lead to unreliable use of the OSPI peripheral. Below is a list of the modifications that were carried out on all E1 versions of the Control Card.

    • Cut the OSPI DQ0 and DQ1 traces on the outside of the vias next to the termination resistors and the mux.
    • Solder a blue wire from R91 to U80 pin 4.
    • Solder a blue wire from R90 to U80 pin 3.
    • Solder one side of the 10kΩ resistor to each of the blue wires added above.
    • Remove R122 and R119.
    • Add blue wire from R91 bluewire 10kΩ resistor to R122 pad closest to U48.
    • Add blue wire from R90 bluewire 10kΩ resistor to R119 pad closest to U48.
  2. CPSW Ethernet Modification - Must be implemented by the user.
Note: This modification was not done to the E1 boards.
Note: This does not apply to E2 versions of the board and beyond.
Note: The board has the PRU0 MII0 signals routed by default to enable CPSW RGMII2. The following modifications need to be followed
Note: The MCAN transceiver and on-board Ethernet cannot be used simultaneously on the E1 version of the AM263Px Control Card.

The E1 AM263Px Control Card had a blue-wire fix to enable the CPSW RGMII2 Gigabit ethernet port with the associated MDIO. The changes are listed below:

  • Routing MDIO0_MDIO to the on-board Ethernet PHY:
    • Remove R208 and solder wire from exposed pad that is not connected to L17 of the SoC to HSEC pin 96.
  • Routing MDIO0_MDC to the on-board Ethernet PHY:
    • Remove R466 and solder wire from R466 pad tied to MCAN1_STB signal.
    • Remove R211 and solder the other end of the MCAN1_STB wire to the R211 exposed pad that is not connected to L18 of the SoC.
  • TCAN1043 Enable driven low
    • Since MCAN1_STB is now routed for MDIO0_MDC, the MCAN transceiver needs to be disabled to avoid any leakage current along the MCAN1_STB trace.