SPRUJ90B March 2023 – February 2024
Each controlCARD comes with a Hardware Developer’s Kit, which is a full set of files necessary to evaluate and develop with a C2000 device. These files include:
The Hardware Developer's Kit for the
controlCARD can also be found in the C2000Ware at the following
location:
- <install
directory>\c2000\C2000Ware_x_xx_xx_xx\boards\controlCARDs\TMDSCNCD28P65X\Rx_x