SPRUJA3 November 2024 F29H850TU , F29H859TU-Q1
The crossbars (XBAR) provide flexibility to connect device inputs, outputs, and internal resources in a variety of configurations. F29H85x contains several XBARs, including Input X-BAR, Output X-BAR, CLB X-BAR, ePWM X-BAR, MINDB X-BAR, and ICL X-BAR. In F29H85x, there is an architectural improvement compared to F28 family. Figure 4-4 shows that the input signals are directed into a MUX, where users can only choose one input within the same MUX. However, Figure 4-5 shows that the inputs are grouped (G0...Gx) instead of muxed, which solves the scenario when users want to select multiple inputs within the same group. Now, they can enable any combination of inputs, even if they are within the same group, to be ORed together to produce the output signal of the X-BAR. This architecture is used across all XBAR modules with the exception of Input X-BAR, which has the same architecture as C28 Input X-BAR.