SPRUJA3 November 2024 F29H850TU , F29H859TU-Q1 , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28378D , TMS320F28379D
The Error Signaling Module (ESM) provides a systematic consolidation of responses to error events throughout the device into one location. The error classification in the ESM is determined by programmed configuration for each individual error input. The module can signal high or low priority interrupts to the processor to respond to an error event and/or manipulate an I/O error pin to signal an external hardware that an error has occurred. This external controller is then able to reset the device and/or keep the system in a safe, known state.