The DC voltage sensing circuit is used to convert the rectified DC bus voltage signal into a low-voltage signal. The circuit is implemented by a low-cost resistor network, as shown in
Figure 2-3. The DC bus voltage can also be used to estimate AC input voltage, as the physical parameters of the AC input circuit are known constants.