SPRUJF4A October 2024 – December 2024
The sensorless FOC structure for an IPMSM is illustrated in Figure 3-12. In this system, the eSMO is used for achieving the sensorless control an IPMSM system, and the eSMO model is designed by utilizing the back EMF model together with a PLL model for estimating the rotor position and speed.
An IPMSM consists of a three-phase stator winding (a, b, c axes), and permanent magnets (PM) rotor for excitation. The motor is controlled by a standard three-phase inverter. An IPMSM can be modeled by using phase a-b-c quantities. Through proper coordinate transformations, the dynamic PMSM models in the d-q rotor reference frame and the α-β stationary reference frame can be obtained. The relationship among these reference frames are illustrated in Equation 20. The dynamic model of a generic PMSM can be written in the d-q rotor reference frame as:
where
By using the inverse Park transformation as shown in Figure 3-13, the dynamics of the PMSM can be modeled in the α-β stationary reference frame as shown in Equation 21:
where
According to Equation 21 and Equation 22, the rotor position information can be decoupled from the inductance matrix by means of the equivalent transformation and the introduction of the EEMF concept, so that the EEMF is the only term that contains the rotor pole position information. And then the EEMF phase information can be directly used to realize the rotor position observation. Rewrite the IPMSM voltage equation Equation 21 as a state equation using the stator current as a state variable:
Since the stator current is the only physical quantity that can be directly measured, the sliding surface is selected on the stator current path:
where