SPRUJF5 November 2024 AM2612
ADVANCE INFORMATION
Flash memory can be utilized two different ways in the user system:
When picking a flash memory IC, the device must comply with all boot requirements of the system-on-chip (SoC). If the memory is used as boot media, some guidelines must be followed to work efficiently as a storage device during application.
Figure 1-1 depicts the flash memory organization once the secondary bootloader (SBL) image and valid application image are present.
Figure 1-2 shows the Boot Flow process where the flash usage is put into perspective, assuming a valid image is already present in flash.