SPRUJF5 November   2024 AM2612

ADVANCE INFORMATION  

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Acronyms Used in This Document
  6. ROM Boot Requirements
  7. Application Requirements
  8. Additional Usage Factors
  9. Flash Support in MCU PLUS SDK
  10. Boot Compatible Flash Devices
  11. Tested Flash Devices
  12. Related Documentation From Texas Instruments
  13. 10Revision History

Additional Usage Factors

Consider the following items when deciding on what flash part to use for the application:

  • What is the flash required for? Some applications require more flash storage than others depending on whether of not the memory is used for booting or storage.
  • Is the entirety of the memory be used? A smaller and lower-cost flash device can be used if a large storage space is not needed.
  • Is the application heavily flash dependent? Typically, 8MB to 16MB is enough for an application, but this varies depending on how heavily external storage is being used.
  • Does the flash part support a RESET signal? If at any point of the application 4-byte addressing mode must be used, then a RESET signal is required to prevent booting problems upon reset.
  • Flash device with RWW support must be used if this function is intended to be used during application