SPRZ457I January   2021  – December 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2287
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2103
      4.      i2184
      5.      i2189
      6.      i2236
      7.      i2185
      8.      i2196
      9.      i2207
      10.      i2208
      11.      i2228
      12.      i2232
      13.      i2244
      14.      i2245
      15.      i2091
      16.      i2235
      17.      i2303
      18.      i2317
      19.      i2134
      20.      i2257
      21.      i2277
      22.      i2285
      23.      i2310
      24.      i2311
      25.      i2313
      26.      i2328
      27.      i2241
      28.      i2279
      29.      i2307
      30.      i2320
      31.      i2329
      32.      i2331
      33.      i2243
      34.      i2249
      35.      i2256
      36.      i2274
      37.      i2278
      38.      i2306
      39.      i2363
      40.      i2312
      41.      i2371
      42.      i2366
      43.      i2138
      44.      i2253
      45.      i2259
      46.      i2283
      47.      i2305
      48.      i2326
      49.      i2368
      50.      i2383
      51.      i2401
      52.      i2409
      53.      i2291
      54.      i2413
      55.      i2414
      56.      i2415
      57.      i2417
      58.      i2418
      59.      i2419
      60.      i2420
      61.      i2422
      62.      i2423
      63.      i2431
      64.      i2433
      65.      i2434
      66.      i2435
  4.   Trademarks
  5.   Revision History

Revision History

Changes from January 1, 2024 to December 2, 2024 (from Revision H (January 2024) to Revision I (December 2024))

  • Added Usage Note i2424; PLL: PLL Programming Sequence May Introduce PLL InstabilityGo
  • Updated Workaround for Advisory i2326; PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limitsGo
  • Added Advisory i2291; Debug: ATB Hang during Cortex-A53 traceGo
  • Added Advisory i2413: Boot: HS-FS ROM boots corrupted ROM boot imageGo
  • Added Advisory i2414: Boot: Ethernet PHY Scan and Bring-Up Flow doesn't work with PHYs that don't support Auto NegotiationGo
  • Added Advisory i2415: Boot: UART Backup Boot Authentication Failure w/ xSPI Primary Boot ModeGo
  • Added Advisory i2417: Boot: GPMC NAND configured to slower clock speedGo
  • Added Advisory i2418: Boot: Secure ROM Panic due to Certificate Info not presentGo
  • Added Advisory i2419: Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabledGo
  • Added Advisory i2420: Boot: XSPI Boot time is not consistent in SFDP modeGo
  • Added Advisory i2422: Boot: ROM timeout for MMCSD filesystem boot too longGo
  • Added Advisory i2423: Boot: HS-FS ROM applies debug access restrictions to all address space covered by the efuse controller firewallGo
  • Added Advisory i2431; BCDMA: RX Channel can lockup in certain scenariosGo
  • Added Advisory i2433: ICSS: Reading the 64-bit IEP timer does not have a lock MSW logic when LSW is readGo
  • Added Advisory i2434: ICSS: IEP RX SOF and TX SOF capture register issue in 32-bit shadow mode when nano seconds part is zeroGo
  • Added Advisory i2435: Boot: ROM timeout for eMMC boot too longGo