SPRZ457I January   2021  – December 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2287
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2103
      4.      i2184
      5.      i2189
      6.      i2236
      7.      i2185
      8.      i2196
      9.      i2207
      10.      i2208
      11.      i2228
      12.      i2232
      13.      i2244
      14.      i2245
      15.      i2091
      16.      i2235
      17.      i2303
      18.      i2317
      19.      i2134
      20.      i2257
      21.      i2277
      22.      i2285
      23.      i2310
      24.      i2311
      25.      i2313
      26.      i2328
      27.      i2241
      28.      i2279
      29.      i2307
      30.      i2320
      31.      i2329
      32.      i2331
      33.      i2243
      34.      i2249
      35.      i2256
      36.      i2274
      37.      i2278
      38.      i2306
      39.      i2363
      40.      i2312
      41.      i2371
      42.      i2366
      43.      i2138
      44.      i2253
      45.      i2259
      46.      i2283
      47.      i2305
      48.      i2326
      49.      i2368
      50.      i2383
      51.      i2401
      52.      i2409
      53.      i2291
      54.      i2413
      55.      i2414
      56.      i2415
      57.      i2417
      58.      i2418
      59.      i2419
      60.      i2420
      61.      i2422
      62.      i2423
      63.      i2431
      64.      i2433
      65.      i2434
      66.      i2435
  4.   Trademarks
  5.   Revision History

i2317

DebugSS: Debug is not available after TRST pin de-assertion when device pin EMU1 is repurposed as MCU_OBSCLK0

Details

The device JTAG port may unexpectedly be connected to the Boundary Scan TAP rather than the On-Chip Debug TAP (SWJ-DP) while using a JTAG debugger when the EMU1 pin is configured for the MCU_OBSCLK0 signal function. This will render the normal JTAG debugging mode inoperable

This occurs because the device selects the Boundary Scan TAP when a value of 01b is sampled on the EMU[1:0] inputs on the rising edge to TRSTn. This value will be driven into the SOC when MCU_PADCONFIG32 is configured for any mux mode value other than mode “0” and MCU_PADCONFIG31 is configured for a mux mode value of “0” with the EMU0 pin pulled high.

  • The EMU1 signal going into the SOC is driven low by the multiplexing logic when the EMU1 signal function is not selected.
  • The EMU0 signal going into the SOC is driven high by internal and external pull-ups.
  • The JTAG debugger de-asserts TRSTn when attempting to communicate with the On-Chip DebugTAP (SWJ-DP).

Workaround

This issue will only occur when the device samples a value of 01b on the SOC EMU[1:0] inputs on the rising edge of TRSTn. This condition can be avoided with any one or more of the following actions.

  • Never connect a debugger to the JTAG port when the EMU1 pin is being used for the MCU_OBSCLK0 signal function.
  • Configure the MCU_SPI0_CS1 pin for the MCU_OBSCLK0 signal function rather than the EMU1 pin, and leave the EMU1 pin in its default configuration.
  • Configure the EMU0 pin to any mux mode other than “0” or “15” when configuring the EMU1 pin for the MCU_OBSCLK0 signal function. This causes the pin multiplexing logic to drive a EMU[1:0] value of 00b into the SOC, which will not select Boundary Scan mode.