SPRZ457I January 2021 – December 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
ICSSG: Device lockup when reading registers in ICSSG module
A device lockup can occur during the second read of any ICSSG register after any MAIN domain power on reset (POR). A MAIN domain POR occurs using the hardware MCU_PORz signal, or via software using CTRLMMR_RST_CTRL.SW_MAIN_POR or CTRLMMR_MCU_RST_CTRL.SW_MAIN_POR. After these resets, the processor and internal bus structures may get into a state which is only recoverable with full device reset using MCU_PORz.
To avoid the lockup, a warm reset should be issued after a MAIN domain POR and before any access to the ICSSG registers. The warm reset realigns internal clocks and prevents the lockup from happening. The warm reset should be triggered using CTRLMMR_MCU_RST_CTRL.SW_MCU_WARMRST. This will issue a warm reset to the entire device (both MCU and MAIN domains), and the device will reinitiate the boot process. Note that reset status bits distinguishing cold and warm resets would not be useful due to this workaround.
If M4F is used as a safety processor, please consult your TI representative for workaround information.
If the application never accesses any ICSSG register, this errata does not apply.